Welcome to Sign in | Join | Help
Not Worth A SFF

In attending last week’s 63rd Annual Texas A&M Instrumentation symposium, I was shocked to hear from a well respected safety expert that SFF (Safe failure fraction) was a failed metric.  No explanation, just that SFF was pretty much useless, followed by a cackle.  I really hate when people make profound statements like this, with no reasoning or justification behind it.  I felt as if the audience was just bullied into this person’s position, and all were just too intimidated to challenge it.  So what’s wrong with SFF?

SFF is defined in ANSI/ISA-84.00.01-2004 Part 1 (IEC 61511-1 Mod), as the fraction of the overall random hardware failure rate of a device that results in either a safe failure or a detected dangerous failure.  It’s sole purpose was to help prevent over optimistic SIL claims by equipment manufactures, and helped to determine the required fault tolerance of your SIS (safety instrumented system). 

While I didn’t get a chance to follow up directly with the individual, I’m pretty sure the argument has something to do with how your system actually responds to a detected dangerous fault.  If your system detects a dangerous fault within itself, does it automatically shutdown your process, or just alarm the operator?  If it’s the latter, than the SFF’s pretty much a failed metric.    

 

Published Wednesday, February 06, 2008 10:12 AM by Charles Fialkowski

Comment Notification

If you would like to receive an email when updates are made to this post, please register here

Subscribe to this post's comments using RSS

Comments

# re: Not Worth A SFF

I favor the SFF. It has not failed, it has saved a few designs. I was asked to review a design where very optimistic failure rate data was being used. The SFF forced the designer to do the right thing by adding a redundant valve in a SIL 3 SIF. Believe it or not, the designer had concluded that only one valve was needed and that a proof test was needed only once pre ten years. I do think we can get rid of this metric some day but not until methods and data become more mature.
Thursday, February 28, 2008 5:07 PM by Bill Goble

Leave a Comment

(required) 
required 
(required)